Configuration, Device Definition Bumpy Confirmation dialog box
Controller operation in multi-controller systems may be affected because a change was made to
the device configuration or the device definition.
You may select
Inhibit Module
to inhibit the device before applying these changes. If
this connection is an Exclusive Owner or Input Only connection and you inhibit the device, any
Listen Only connections from other controllers cannot open until the connection is
re-established (preventing them from misinterpreting data received from the newly reconfigured
device.)- SelectYesto apply the changes. This may affect other controllers.
- SelectNoto return to the editing session (any profile changes are pending).
Provide Feedback