Bumpy Confirmation dialog box

The connection to the device is disabled due to a change in the:
  • Requested Packet Interval (RPI)
  • Electronic Keying
  • Minor Revision
  • Device Definition
  • Device Configuration
  • Inhibit the device Connection
  • Input Type
  • Input Trigger
Apply the change:
  • Select
    Yes
    . The device connection is interrupted to apply the change. If the Inhibit option is selected, the connection is inhibited.
  • Select
    No
    to return to the previous editing session (any profile changes are pending).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal