Configure individual input point properties

Configure the properties of the individual input point to eliminate high frequency oscillations or spikes from input signals for that point.
To configure individual input point properties
  1. On the tab for the device, expand
    Points
    , and then select an individual point.
  2. In the
    Ptxx
    view, fill in the parameters and select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal