Configure individual output channel properties

Configure the individual output channel so that it can properly connect to Current or Voltage output types and to multiple output signal ranges.
To configure individual output channel properties
  1. On the tab for the device, expand
    Channels
    , and then select an individual channel.
  2. In the
    Ch0x
    view, fill in the parameters and select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal