Calibration Wizard parameters

Calibration Wizard
includes these parameters:
Parameter
Description
Channel
Shows the channel number to which this configuration applies.
Calibrate
Identifies the channels for calibration.
Select the checkbox for the channel that you want to calibrate.
Calibration Range
Shows the value currently configured for the channel.
  • 0 mA to 20 mA
    when
    Input Type
    is Current.
  • -10 V to 10 V
    when
    Input Type
    is Voltage.
Calibration Gain
Shows the calibration gain values as reported by the device.
Calibration Offset
Shows the signed values as reported by the device.
Calibration Status
Shows the status of the calibration per channel as the calibration occurs.
Low Reference
Shows the value of the low reference signal for the channel.
High Reference
Shows the value of the high reference source based on the channel configuration.
Recorded Reference
Indicates the measured output values.
For the multimeter accuracy, see the User Manual.
Status
Shows the value read during calibration for the enabled channels.
  • OK
    - Indicates that the reference signal is within the acceptable range.
  • Error
    - Indicates that the reference signal is not within the acceptable range.
If
Status
shows
Error
, perform the corresponding actions as needed:
  • For output devices, measure and enter the recorded reference values again for the channels in error, and then select
    Retry
    .
  • For input devices, investigate the channels with errors, and then select
    Retry
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal