Calibration mismatch

Performing calibration can cause unexpected results if:
  • At least one channel is selected, and
  • There is a mismatch between the device listed in the application and the actual physical device, and
  • The system is active.
It is strongly recommended that you select
No
, check the configuration, and shut down the system before performing calibration.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal