Loading
Press Release | August 13, 2024

Rockwell Automation and Building Material Company Cimento Itambé Optimize Predictability and Energy Usage in Cement Production

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
  • Cement Facility
    Process control for cement companies is complex. Model predictive control can help increase equipment uptime and reduce energy use.

Cement production has its challenges—notably, the variability of resources can make kilns difficult to control and manage. Cimento Itambé wanted to optimize kiln productivity, increase mill productivity, and reduce energy use.

Rockwell Automation (NYSE:ROK) worked with Cimento Itambé to implement model predictive control (MPC) technology. MPC allowed Cimento Itambé to standardize operational processes, gain more equipment availability, and use less energy in their cement manufacturing process.

The first phase of the project, targeting the kilns, was completed in late 2022. During this phase, Cimento Itambé experienced a 5% increase in productivity, a 2% reduction in energy use in each kiln, and overall, more stable temperatures.

The second phase, improving the grinding operations, was completed in 2023. During this phase, Cimento Itambé realized a 5% reduction in energy usage, a 5-10% increase in productivity, and fewer disruptions in feeding or stops related to high vibrations.

Learn more about how MPC technology can put cement plants on the path to more stable production, reduced energy usage, and higher throughput.

Published August 13, 2024

About Rockwell Automation

 
 

Rockwell Automation, Inc. (NYSE: ROK), is a global leader in industrial automation and digital transformation. We connect the imaginations of people with the potential of technology to expand what is humanly possible, making the world more pr oductive and more sustainable. Headquartered in Milwaukee, Wisconsin, Rockwell Automation employs approximately 26,000 problem solvers dedicated to our customers in more than 100 countries as of fiscal year end 2025. To learn more about how we are bringing the Connected Enterprise® to life across industrial enterprises, visit www.rockwellautomation.com.

About the Rockwell Automation PartnerNetwork

Rockwell Automation believes we're better together—and we do our part by delivering an expansive, global partner ecosystem of market-leading technology, superior support and services, and an integrated and streamlined approach to business. Succeed on an international scale by utilizing our network's breadth of innovative technologies and services that no single vendor can provide alone. To learn more about how the PartnerNetwork is helping to deliver the value of The Connected Enterprise, visit PartnerNetwork Program.


  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Press Releases
  5. Chevron LeftChevron Left Rockwell Automation and Building Material Company Cimento Itambé Optimize Predictability and Energy Usage in Cement Production