Electronically modeled and defined in the MES, IPC activities help improve product quality and minimize human error
MILWAUKEE, Oct. 23, 2014 — In-process control (IPC) checks are essential in the highly regulated life sciences industry. However, manually conducting IPC checks can introduce human error, while standalone IPC systems are difficult to integrate with electronic batch records. Rockwell Automation has added new recipe modeling capabilities to its Rockwell Software PharmaSuite v6.0 manufacturing execution system (MES) to help streamline these crucial activities into the larger production and packaging processes.
Throughout the design process, the building block library within the PharmaSuite recipe designer allows programmers to re-use and maintain modeled IPC checks across multiple recipes.“This latest version of PharmaSuite software further extends pharmaceutical manufacturers’ IPC capabilities,” said Martin Dittmer, PharmaSuite product manager, Rockwell Automation. “IPC quality checks that previously were the sole responsibility of an operator can now be easily defined and modeled into the recipe up front in the MES, providing instructions, data collection and alerts to ensure these activities are carried out.”
Within a running program, escalation management helps monitor, control and log the timely execution of IPC checks through an escalating series of documented alerts. For example, a quality check that must be conducted within a five-minute time frame every 30 minutes will first alert the operator when the five-minute window arrives. A warning is provided if the activity is not completed after a set time. The activity data, including any exceptions or deviations, is recorded and logged in the batch record for the quality assurance team to review and take action on, if necessary.
Added Work-Flow Flexibility
PharmaSuite v6.0 software also incorporates new work-flow integration capabilities, allowing executed work-flow information to be appended and tracked as part of the electronic batch record.
Typically when using other systems, an operator must manually create and attach new paper documentation for any additional work flow. However, this process can be time consuming and riskier due to human error. Pre-defined work flows can be created up front in PharmaSuite v6.0 software, and then operators can select, execute and document the work flow as needed during production. This also provides a new level of flexibility on the plant floor, creating an opportunity to streamline the content of master recipes.
Additionally, new re-work capabilities introduced in PharmaSuite v6.0 software offer greater MES flexibility, enabling operators to abort and re-activate a production process. These new capabilities eliminate the time, cost and effort of completely re-starting an order from the beginning should an unexpected issue arise, while also ensuring the re-work activities are carried out in a controlled and documented fashion.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs about 22,000 people serving customers in more than 80 countries.
Media Contacts
Paula Puess
Rockwell Automation
440.646.3806
pdpuess@ra.rockwell.com
pdpuess@ra.rockwell.com
Anne Neubauer
PadillaCRT
612.455.1918
anne.neubauer@padillacrt.com
LISTEN. THINK. SOLVE., PharmaSuite and Rockwell Software are trademarks of Rockwell Automation Inc.
Published October 22, 2014