From Teledyne DALSA
Editor’s Note: This article is adapted from the white paper, “A Close Look at Vision Guided Robotics (VGR).” Download the full white paper that describes ideal manufacturing environments and applications for VGR in industries such as medical device, pharmaceutical, food packaging and agriculture; explains how machine vision and robotics combine using hardware and algorithms to create VGR; and provides a real-world case study.
We’ve all seen videos of robots rapidly assembling cars with little or no human intervention. Industrial robots like these have increased productivity in almost every manufacturing sector, but they have one shortcoming: they can’t “see.”
Programmed to repeat exactly the same motions over and over again, they can’t detect and maneuver objects of different shapes, sizes and colors, or objects that touch and overlap. So, if a product changes or is added to the production line, the robots must be reprogrammed. And if product components are delivered to the line by traditional hoppers and shake tables, bowl feeders must be retooled.
Beyond Repetitive Tasks
A new generation of robots guided by advanced machine vision is taking robots beyond repetitive tasks. Fueled by smaller, more powerful and less expensive machine vision cameras and other vision sensors, increasingly sophisticated robotic algorithms and processors with machine vision-specific hardware accelerators, these vision guided robot (VGR) systems are transforming manufacturing and fulfillment processes.
VGR makes robots highly adaptable and easier to implement for industries in which new products are introduced frequently and production runs are short, including medical device and pharmaceutical manufacturing, food packaging, agricultural applications, life sciences and more.
What About 3D Vision?
Often, VGR systems use more than one type of sensor to build 3D images. For example, a robot with a 3D area sensor locates and picks randomly positioned parts in a bin. Then a 2D camera detects the orientation of each part on the fly, so that the robot can correctly place them on a conveyor.