Convert a Standalone Chassis to a Redundant Chassis Pair
To convert a standalone chassis to a redundant chassis pair, follow these steps. For details about how to convert from a non-redundant system, see Convert from a Non-redundant System.
- Insert a redundancy module in a spare slot in the standalone chassis.
- Configure an identical chassis with compatible modules in the same slot as the standalone chassis.
Provide Feedback