Monitor and Maintain Redundancy

To monitor and maintain redundancy, you can do the following:
  • Reference the controller log
  • Track changes to components, such as routines and Add-On Instructions
  • Use logic to monitor status
  • Monitor communication module statistics
  • Understand temperature monitoring and fault behavior
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal