Configure Front Port Crossload Security

When Front Port Crossload mode is enabled, front port crossload security enables secure crossloading of data via the front Ethernet ports of redundant controllers.
Front Port Crossload Security Enabled Checkbox
Front Port Crossload Security Enabled Checkbox
IMPORTANT:
Front port crossload security is enabled by default and can cause slower system performance, such as degraded scan time and qualification time. However, the switchover time is not affected.
To avoid impact to system performance, you can disable the feature.
You can enable or disable front port crossload security only when the controller is in a disqualified state. The controller can be offline or online.
Whenever this setting is changed, an event is logged in the controller event log.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal