Requirements for Data Confidentiality
Security Component | Required to Meet IEC‑62443-4-2 SL 1 | Details |
|---|---|---|
FactoryTalk® Security software | Yes | Configure FactoryTalk® Security to define policies, user groups, and other permission sets.
For more information, see Configure System Security Features User Manual, SECURE-UM001 . |
FactoryTalk® Policy Manager software | Yes | Use the FactoryTalk® Policy Manager software to define a secure data transport over an EtherNet/IP™ network to the controller.For more information, see Configure System Security Features User Manual, SECURE-UM001 . |
License-based source and execution protection | May be required based on system design, threat model, and risk assessment. | Configure licenses to manage access to controller source logic and execution of that logic. These licenses are not enabled by default.
For more information, see License-based Source and Execution Protection. |
Access to tag data | May be required based on system design, threat model, and risk assessment. | Configure the following attributes in the Logix Designer application to control access to tag data:
|
SD card encryption | May be required based on system design, threat model, and risk assessment. | If your system allows for microSD memory card use, the load process to the memory card encrypts and digitally signs the project by using the controller key. The memory card itself is not encrypted. When you save (load) firmware to the memory card, the process stores encrypted firmware and certificates on the memory card. Do not use a Message to Self (MSG with a Path of THIS) to auto-write controller logs or manually force a write of controller logs to the memory card. This can help prevent against potential loss of controller logs before FactoryTalk® AssetCentre can read them.For more information, see Use the Memory Card. |
Provide Feedback