Safety Signature Hierarchy
    The following image shows an example of the safety signature hierarchy:
- A signature with ID and time stamp exists for each element in the hierarchy.
 - Expand the safety signature at the top to view its underlying elements.
 - Expand a parent element to view its underlying child elements.
 
Safety Signature Hierarchy
Item  | Description  | 
|---|---|
A  | Safety signature  | 
B  | Safety signature elements  | 
Aggregate Signatures
      Safety elements that include a collection of tags and parameters have aggregate signatures. An aggregate signature represents the validity of all tags and parameters within the element.
The following elements have aggregate signatures:
- Controller-scoped safety tags
 - Safety program parameters and tags
 - Safety Add-On Instructions
 - Safety mapped tags
 - Safety I/O connections
 
If one of the preceding elements has a collection with no members, such as no controller-scoped safety tags, the aggregate signature value appears as 64 zeros.
Provide Feedback