Safety Applications
    The safety concept assumes the following requirements:
- You are responsible to create, operate, and maintain the safety application.
 - You are fully qualified, specially trained, and experienced in safety systems.
 - You apply the logic correctly to detect programming errors through strict adherence to specifications, programming, and naming rules.
 - You perform a critical analysis of the application and use all possible measures to detect a failure.
 - You confirm all application downloads via a manual check of the safety signature.
 - You perform a complete functional test of the entire system before the operational startup of a safety-related system. This test includes, but is not limited to, the following:
- Validate that the overall functionality of the implemented safety functions, including I/O configuration via Add-On Profiles, beyond the limits of the individual devices (boundary testing).
 - Verify that the correct versions of software are used.
 
 
Controller Mode  | Controller Safety Execution  | 
|---|---|
Program  | 
  | 
Test  | 
  | 
Run  | 
  | 
Unlocked no signature  | Only for development purposes  | 
  | 
Locked no signature  | Only for development purposes  | 
  | 
Unlocked with signature  | SIL 2/SIL 3 (per controller)  | 
  | 
Locked with signature  | SIL 2/SIL 3 (per controller)  | 
 
     IMPORTANT: 
    If the controller is safety-locked and the safety-unlock password is lost and a download is needed, you must perform a Stage 1 reset of the controller. 
 | 
Provide Feedback