Create Signature History Entry
    The signature history provides a record for future reference. A signature history entry consists of the instruction signature, the name of the user, the time stamp value, and a user-defined description. Up to six history entries can be stored. You must be offline to create a signature history entry.
     TIP: 
    The Signature Listing report in the 
Studio 5000 Logix Designer®
 application prints the instruction signature, the time stamp, and the safety instruction signature. To print the report, right-click Add-On Instruction in the Controller Organizer and choose Print > Signature Listing.Provide Feedback