Logix System Reaction Time
    The following sections provide information on how to calculate the Logix system reaction time.
Simple Input-Logic-Output Chain
      This section describes the Logix system reaction time for any simple input-logic-output chain.
Worst Case Reaction Time
The Logix system reaction time for any simple input to logic to output chain consists of the following components.
Item  | Description  | 
|---|---|
A  | Safety input device reaction time plus input delay time, if applicable.  | 
B  | Safety input connection reaction time limit. Read from the Module Properties dialog box in the Logix Designer application, this value is a multiple of the safety input device connection RPI.  | 
C  | Controller reaction time. See Safety Task Reaction Time.  | 
D  | Safety output connection reaction time limit. Read from the Module Properties dialog box in the Logix Designer application, this value is a multiple of the safety task period.  | 
E  | Safety output device reaction time.  | 
Logic Chain Using Produced/Consumed Safety Tags
      This section describes the Logix system reaction time for any input to controller A logic to controller B logic to output chain.
Reaction Time with Produced/Consumed Safety Tags
The Logix system reaction time for any input to controller A logic to controller B logic to output chain consists of the following components.
Item  | Description  | 
|---|---|
A  | Safety input device reaction time plus input delay time, if applicable  | 
B  | Safety input connection reaction time limit   | 
C  | Safety task period plus safety task watchdog time for controller A  | 
D  | Produced/consumed safety connection reaction time limit  | 
E  | Safety task period plus safety task watchdog time for controller B  | 
F  | Safety output connection reaction time limit  | 
G  | Safety output device reaction time  | 
Provide Feedback