Important User Information
    Read this document and the documents listed in the additional resources section about
        installation, configuration, and operation of this equipment before you install, configure,
        operate, or maintain this product. Users are required to familiarize themselves with
        installation and wiring instructions in addition to requirements of all applicable codes,
        laws, and standards.
Activities including installation, adjustments, putting into service, use, assembly,
        disassembly, and maintenance are required to be carried out by suitably trained personnel in
        accordance with applicable code of practice.
If this equipment is used in a manner not specified by the manufacturer, the protection
        provided by the equipment may be impaired.
In no event will Rockwell Automation, Inc. be responsible or liable for indirect or
        consequential damages resulting from the use or application of this equipment.
The examples and diagrams in this manual are included solely for illustrative purposes.
        Because of the many variables and requirements associated with any particular installation,
        Rockwell Automation, Inc. cannot assume responsibility or liability for actual use based on
        the examples and diagrams.
No patent liability is assumed by Rockwell Automation, Inc. with respect to use of
        information, circuits, equipment, or software described in this manual.
Reproduction of the contents of this manual, in whole or in part, without written
        permission of Rockwell Automation, Inc., is prohibited.
Throughout this manual, when necessary, we use notes to make you aware of safety
          considerations.
    
    
    
    
    
    
     WARNING: 
    
Identifies information about practices or circumstances that can cause an explosion in
            a hazardous environment, which may lead to personal injury or death, property damage, or
            economic loss.
     ATTENTION: 
    
Identifies information about practices or circumstances that can lead to personal
            injury or death, property damage, or economic loss. Attentions help you identify a
            hazard, avoid a hazard, and recognize the consequence.
     IMPORTANT: 
    
Identifies information that is critical for successful application and understanding of
            the product.
These labels may also be on or inside the equipment to provide specific precautions.
    
    
    
    
    
    
     SHOCK HAZARD: 
    
Labels may be on or inside the equipment, for example, a drive or motor, to alert
            people that dangerous voltage may be present.
     BURN HAZARD: 
    
Labels may be on or inside the equipment, for example, a drive or motor, to alert
            people that surfaces may reach dangerous temperatures.
     ARC FLASH HAZARD: 
    
Labels may be on or inside the equipment, for example, a motor control center, to alert
            people to potential Arc Flash. Arc Flash will cause severe injury or death. Wear proper
            Personal Protective Equipment (PPE). Follow ALL Regulatory requirements for safe work
            practices and for Personal Protective Equipment (PPE).
The following icon may appear in the text of this document.
    
    
     TIP: 
    
Identifies information that is useful and can help to make a process easier to do or
            easier to understand.
Rockwell Automation recognizes that some of the terms that are currently used in our
        industry and in this publication are not in alignment with the movement toward inclusive
        language in technology. We are proactively collaborating with industry peers to find
        alternatives to such terms and making changes to our products and content. Please excuse the
        use of such terms in our content while we implement these changes. 
Provide Feedback