Understanding Event Messages
    Syslog event messages fall within groups as listed and defined in the table below.
Additional information for specific event messages is located in SYSLOG-RD001.
Event Message Group  | Definition  | 
|---|---|
Auth  | An account management-related event  | 
Backup  | A general backup or restore related event  | 
CIP Sec  | A  CIP Security™ -related event | 
Config  | A general configuration-related event  | 
Ctlr  | A Programmable Automation Controller related event  | 
Discovery  | A system discovery-related event  | 
Log  | A log-related event  | 
Safety  | A  CIP Safety™ -related event | 
Sys  | A general system-related event  | 
HTTP  | A web server or client-related event  | 
CIP  | A  CIP™ -related event | 
Provide Feedback