Failed to modify the properties for the routine
This error occurs when trying to apply the edits on the Routine Property dialog box. This can occur because:
- Bad IEC name. Enter a name that adheres to the IEC-61131 naming standard.
- Out of memory
Provide Feedback