Connection configuration options
TIP:
To open the
Connection Configuration
dialog:- In the Tag Editor'sConnectioncolumn, put the cursor in the cell of the connection you wish to view and then select the Browse
button.- Or - - In theTag Propertiesdialog, select theOpen Parameter Connectionscheck box.
Use the grid table provided in the
Connection Configuration
dialog to view, create, delete, and modify connections between parameters, controller scoped tags, and their members. The Connection Configuration
dialog is helpful for viewing and configuring multiple connections. The leftmost part of the grid provides an icon that indicates the condition of the connection:
Icon | Description |
* | Row in which content changed and the change is not saved. |
Row with error in the content. Fix the error before downloading the project to the controller. | |
Row in which to create a connection. |
Use the keyboard to navigate in the
Parameters and Connections
grid.This table describes the settings on this dialog:
Setting | Description |
Name | Shows the name of the connection endpoint. You have the option to edit the name of the connection endpoint. If you want to create a connection, locate the create icon |
Usage | Shows the usage type (Local, Input, Output, InOut, Public, or <controller>) of the connection endpoint.
IMPORTANT:
A single part (member, element, or bit)
of a program’s Input parameter cannot have multiple connections.
|
Data Type | Shows the data type of an endpoint tag or structure member. |
Alias For | If an endpoint tag is an alias, this column shows the target tag (the tag that contains the datatype definition for an alias tag). These attributes of the alias tag are copied from its base tag:
|
Base Tag | Shows the last link in an alias chain. This is the tag that contains the datatype definition. |
Description | Contains the description, if any, for each endpoint tag or structure, array, or bit member. If pass-through descriptions are enabled and an explicit description for a tag is not provide, one of these options occurs:
If supplied, a description for the selected item appears in this column. |
External Access | Indicates whether the endpoint tag has Read/Write, Read Only, or no access (None) from external applications such as HMIs. |
Constant | Indicates whether logic is prevented from writing values to the associated endpoint tag or parameter. If a logic routine tries to write to a constant tag, the routine will not verify. |
Provide Feedback