Failed to retrieve the contents of the rung for rung # <Rung Number>

Internal Error: The Ladder Editor tried to read a rung from the project file, but the operation did not succeed. This could occur because:
  • the rung number is invalid
  • there was insufficient memory
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal