New Routine Dialog Box Overview

Enter the information necessary to create a new routine from this dialog box.
Parameters
Name
Enter a name for the routine.
Description
Enter a description of the routine.
Type
Select the type of routine from the pull-down menu. Choose from:
  • Ladder Diagram
  • Sequential Function Chart
  • Function Block Diagram
  • Structured Text
In Program or Phase
Select the program or phase to which the routine will belong.
Assignment
Select the assignment for the routine: <none>, Main, Fault or Prestate.
Class
Indicates whether the routine is a Standard routine or a Safety routine. This value applies to Safety applications only.
Open Routine
Select this box if you want the routine to open in the appropriate editor once you have created it.
OK
Select this button to accept the information you have entered and create the new routine.
TIP:
If you are online, the routine is created in the controller.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal