Not enough hard disk space for trend log file

The trend started and the hard drive is about 80 percent full, or has 100 MB of space left. Either clear additional space on the hard drive or stop and close the trend, reopen it, and reconfigure it to use less hard disk space.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal