(Interactive Access) Processes
    This section shows a list including all the ongoing processes. They can be stopped by clicking the 
End processes
 button.FactoryTalk®
          Remote Access™
 ManagerProcesses
        Manager
 to assist in identifying running processes on remote devices, CPU usage
      percentage and memory usage.To access 
Processes Manager
, proceed as follows:- Make sure that theis connected to the remote device.FactoryTalk® Remote Access™Manager
- Access .Or.NOTE: TheProcessesfeature cannot be accessed throughInteractive Access (Web only).
- TheEnd processesbutton activates.NOTE: Use theEnd processesbutton to end any process, as needed.
Provide Feedback