Router factory settings and identification
    The following table shows the factory settings of router interfaces:
| Interface | IP Address | Mask | 
| LAN | 192.168.0.1 | 255.255.255.0 | 
| WAN | DHCP | 
The router settings configuration is protected with user/password credentials.
      
- The default (not changeable) user isadmin.
- The default password (configurable) isadmin.
Factory settings information is located on the router side, together with the MAC addresses of both LAN and WAN network interfaces.
Provide Feedback