Protection against domain change
    Stratix®
          4300
 Remote AccessFactoryTalk®
          Remote Access™
 ManagerThis means that the device registration domain cannot be changed, since the registration information is stored on the server once the device is registered. For this reason, the device is registered to the domain until it will be completely removed from the same.
     NOTE: 
    See Device move and removal for further information on this subject.
In case of non-authorized domain change attempt, a security block triggers, preventing the router from being registered to a domain and the 
Device Registration
 Tool will return an error message.Restore Operation
      To restore the router operation after a security block, contact the Technical Support Team.Provide Feedback