Reference Architectures Overview
FactoryTalk® Optix™
is a visualization platform that helps improve user
process, efficiency, and deliverables – in one tool. Take advantage of new levels of
collaboration, scalability, and interoperability to achieve their HMI vision.Modular deployment enables deploying only what is needed to the runtime application. This
feature supports scaling of the hardware platform, opening up new options for IIoT and Edge
visualization, connectivity, and analytics.
Provide Feedback