View instances of a type

View instances of a type, such as a window, to view all of the places in the information model the type exists. View instances of a type from
Project view
.
  1. In
    Project view
    , navigate to and right-click the type and then select
    Show Instances
    .
  2. In
    Instances of (name)
    , select an instance of the type and select
    Go to ...
FactoryTalk Optix Studio
navigates to the instance of the type in the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.