Configure a client device
Configure a client device to enable
FactoryTalk Optix Studio
to deploy the FactoryTalk Optix Application
to the client. The FactoryTalk Optix Application
can be deployed to a client device either over the network or by exporting the FactoryTalk Optix Application
to a folder or USB drive.- SelectRunto display the pull-down menu and then selectConfigure target device. TheDeployment target device configurationwindow opens.
- SelectAdd
to add a client device, then fill in the available fields.
- InName,enter a name for the target device.
- InIP Address, enter the IP address of the client device.
- InUsername, enter the user account used to connect to the client device:
- Windows client device: the username must be a system user name.
- DOMAIN\Username, for domain users
- .Username, for local users on domain-joined devices
- Username, for local users on devices that do not belong to a domain
- Linux client device: the username must be that of the admin user.
- (optional). Only for Windows client devices -- in theDestination path, type the path on the target in which to transfer the application, if the transfer is not to be in the predefined path (in %localappdata%, on partition C).TIP: Specify a different path when the C partition on the client device is write-protected.
Provide Feedback