OMRON Fins Driver

Driver to communicate with the OMRON Fins PLC.
BrowseName
OmronFinsDriver
SuperType
Communication driver(CommunicationDriver)

Properties

Name
BrowseName
DataType
Description
Station ID
StationID
Destination Network Address
DestinationNetworkAddress
Default value = 0. It corresponds to the FINS parameter named Network Address. It can be set to 0 if the PC and all the devices are on the same network. If there are more network levels, using gateway devices, you should specify the network number (valid value are in 1-127 range).
Destination Node Address
DestinationNodeAddress
Default value = 0. Correspond to the FINS parameter Node address. It depends on the FINS net configuration. Usually it corresponds to the last octet of the PC Ethernet card IP address, i.e. if 192.168.0.38 is the PC IP address, use 38 as node number.
Destination Unit Address
DestinationUnitAddress
Default value = 0. It corresponds to the FINS parameter named Unit Address. Should be left to zero.
Protocol
Protocol
Protocol mode: Ethernet or serial
Serial port
SerialPort
Baudrate
Baudrate
Data size
DataSize
Parity
Parity
Stop bits
StopBits
Flow control
FlowControl
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.