AuthenticationMode
- BrowseName
- AuthenticationMode
Values
Value | DisplayName | Description |
---|---|---|
0 | Model only | (default) Allows only the users created in FactoryTalk Optix to log in. |
1 | Local only | Allows only local Windows users to log in. |
2 | Domain only | Allows only Active Directory users to log in. |
3 | Domain and local | Allows only Active Directory users and local Windows users to log in. |
4 | Any | Allows users of any type to log in. |
Provide Feedback