Configure the speed panel (type)

Add a label, gauge, and a button that changes panels.
  1. Create a speed label:
    1. In
      Project view
      pane, right-click
      SpeedPanel (type)
      and select
      New
      Base controls
      Label
      .
    2. Hover-over the label, select
      Edit
      , and enter
      SpeedLabel
      .
    3. In
      Properties
      pane, set
      Text
      to
      Speed
      .
  2. Create a speed circular gauge:
    1. In
      Project view
      , right-click
      SpeedPanel (type)
      and select
      New
      Base controls
      Circular gauge
      .
    2. Hover-over the label, select
      Edit
      , and enter
      SpeedGauge
      .
    3. In
      Properties
      , create a dynamic link between
      Value
      and
      ProjectName
      Model
      Acceleration
      .
      For more information about dynamic links, see Create dynamic links.
  3. Create a button that changes panels:
    1. In
      Project view
      , right-click
      SpeedPanel (type)
      and select
      New
      Base controls
      Button
      .
    2. Hover-over the label, select
      Edit
      , and enter
      ChangePanelButton
      .
    3. In
      Properties
      , set the
      Text
      property value to
      Change Panel
      .
    4. In
      Events
      , next to
      MouseClick event
      , select
      Add
      and select
      Panel Loaders
      {MainPanelLoader}
      MainPanelLoader
      Change panel
      .
    5. Under
      Input arguments
      , create a dynamic link between
      NewPanel
      and
      ProjectName
      UI
      RemotePanels
      SpeedPanel (type)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.