Edit task properties
Use the
Properties
pane to edit the properties of existing tasks. - On the explorer bar, select
Execution. - Expand the folder of the controller.
- Expand theTasksfolder and select the task.
- InPropertieson theConfigurationtab, configure the task:
- Type. SelectEvent,Continuous, orPeriodic.For an explanation of task types and when to use them, see the Logix 5000 Controllers Tasks, Programs, and Routines Programming Manual.
- Period. Enter the frequency to perform the task. Reducing the Period rate increases how often the task performs. Increasing the frequency causes other tasks in the controller to perform at a slower rate.
- Priority. Enter the priority level of the task. Lower numbers indicate higher priorities for tasks. A task assigned a 1 is a higher priority task than a task assigned a 15.
- Watchdog. Enter the maximum time in milliseconds the task can run before triggering a motor control fault.IMPORTANT: For safety tasks, enter a watchdog less than or equal to thePeriodrate.
- (optional)Disable automatic output processing to reduce task overhead. Position the switch to
Onto help prevent external output modules from updating the data table values of the controller at the end of the task scan. Position the switch to
Offto enable updates. - (optional)Inhibit task. Position the switch to
Onto help prevent the controller from performing this task. Position the switch to
Offto enable the controller to perform this task.
- InProperties, select theProgram Scheduletab and configure the schedule:
- UnderScheduled, drag and drop programs in the list to change the execution order of the programs.
- UnderUnscheduled, drag and drop programs into theScheduledlist.
- SelectApply.See Task example for a description of the syntax required to create a task in the FactoryTalk Design Studio Code editor.
Provide Feedback