Delete a routine
Delete a routine to remove it from the program.
IMPORTANT:
If the routine is the Main routine or Fault routine of the program, before deleting the routine, edit the program properties to disassociate the routine from its function in the program.
- On the explorer bar, select
System. - InSystem, expand theFactoryTalk Smart Objectand program.
- Right-click the routine to delete and selectDelete. The messageAre you sure you want to delete this routineappears.
- SelectDelete. The routine is removed.
Provide Feedback