Pull changes from the remote repository
Update your local workspace when changes are made to the remote repository. Pull changes when the status bar displays
Remote changes available
. When you pull changes, the project copy in your local workspace is updated with changes made to the project in the remote repository. Any conflicts between the two versions of the project appear for you to choose which version of a change to keep.
IMPORTANT:
Pulled changes cannot be undone. Pull changes only if you want to make the project in your local workspace the same as the project in the remote repository.
TIP:
The number in the icon identifies the total commits made by other users sharing the project (remote commits).
Prerequisite
- If you made changes to the local project, commit your changes before pulling remote commits. Select
Commit. In the open project, ifRemote changes availableappears in the status bar, select
Pullor selectFile > Source control > Pull. The open project updates with any changes made to the shared project on the remote repository.TIP: If the remote version of the project has changes to the same content as the local project version,Manage conflictsopens.
To pull changes from the remote project
:- IfManage conflictsopens, use:
- Statusto identify if the file contains conflicts.
- Pathto reference the files that have conflicts.
- Conflictsto identify the number of conflicts in a file andTotal conflictsto identify all the known conflicts.
- Select each conflict in the table and then select an option above the changed code for the conflict:
- Accept local change. Discard the change made to the remote version of the project and accept the change that appears in the LOCAL CHANGES row of code. This option updates the remote version of project with the change made to the local version of the project.
- Accept remote change. Discard the change made to the local version of the project and accept the change that appears in the REMOTE CHANGES row of code. This option updates the local version of the project with the change made to the remote version of the project.
- Accept both changes. Apply the changes in both the LOCAL CHANGES and REMOTE CHANGES rows of code.TIP: If another user deletes a file remotely from the shared project whileManage conflictsis open,Remote changes availableappears again.
- (optional) After you accept changes, theRevertbutton is enabled. SelectRevertif you want to return the files to the previously applied or committed changes.
- To manage any remotely removed files, select
Pullagain and then in the firstKeep filecolumn ofManage conflicts, either:- Select the checkbox to keep the file that the other user removed remotely.
- Leave the checkbox cleared to remove the file from your local project as well.
- When all conflicts are resolved, selectAccept.
Provide Feedback