Create FaultHandler program
Create a program to operate as the controller fault handler. Program tags are automatically created when you create a FaultHandler program.
- On the explorer bar, select
Execution. - Right-click theHandlersfolder and selectNew FaultHandler program.
- InNew Programconfigure:
- Name. Read-only.
- Description. Enter a description of the program.
- Create a Main Routine. Position the switch
to On. - Main Routine type. SelectLadder Diagram.
- SelectCreate. The new program and main routine appear inSystem.
Provide Feedback