View a device profile
View a device profile to view and edit device settings such as connections, ports, and electronic keying.
TIP:
If you are online, the profile will open in read-only. You can use the offline icon to open the offline version of the profile.
- On the explorer bar, select
Devices. - InDevices, selectDevice list.
- InDevice list, right-click the device, then selectOpen device properties.
Provide Feedback