Unassign a device
Unassign a device to remove its association with a parent device. When you unassign a device, all its connections are removed from the project and the device moves to the Unassigned folder as an existing device.
TIP:
Any changes made to devices while online will only impact the offline project.
TIP:
To reassign a device, see Add an existing device.
Unassign devices from the
Devices
explorer.
- On the explorer bar, select
Devices. - SelectInDevicesexplorer, right-click the device and selectUnassign.Unassignin the confirmation dialog. The device moves to theUnassignedfolder.
NOTE:
When you unassign a device, the devices assigned to it become unassigned, and on rack optimized devices, the device connection type reverts to the default setting, Data.
Provide Feedback