Monitor ethernet node capacity
In
Properties
, use the information in Ethernet Nodes Capacity
to monitor controller ethernet node usage.- On the explorer bar, select
Devices. - InDevices, select the controller.
- IfPropertiesis not open, on the pane bar, select
Properties. - InProperties, underEthernet Nodes Capacity, monitor the controller memory usage. TheEthernet Nodes Capacitypane indicates the available nodes, used nodes, and total capacity.If the size of the project approaches or exceeds the total ethernet nodes capacity available in the controller, a message warns you about the limited or exceeded capacity. When the ethernet nodes capacity is exceeded, you cannot deploy to any controller types except ControlLogix 1756-L85 controllers.TIP: In the Execution explorer, click on the controller to view the Properties.
Provide Feedback