Monitor controller capacity
In
Properties
, use the information in Controller Capacity
to monitor controller memory usage. To monitor controller capacity:
- On the explorer bar, select
Devices. - InDevices, select the controller.
- IfPropertiesis not open, on the panebar, select
Properties. - UnderController Capacity, monitor the controller memory usage. The Controller Capacity pane indicates the used and unused blocks on the controller. Blocks represent units that consume the controller’s memory.If the size of the project approaches or exceeds the total capacity available in the controller, a message warns you about the limited or exceeded capacity. When the controller capacity is exceeded, you cannot download to the controller.Monitor these capacity indicators:
- Usage. Shows the percentage of blocks used by the project.
- Available. The number of unused blocks.
- Used. The number of blocks used by the project.
- Total. The total number of blocks available in the controller.
TIP:
In the Execution explorer, click on the controller to view the Properties.
Provide Feedback