Export Stratix device configuration
Export a
Stratix
device configuration to back up a device configuration to a computer. The configuration contains either one or two configuration files.- On the explorer bar, select
Devices. - InDevices, right-click aStratixdevice, and then selectProperties.
- InProperties, selectSave/Restore, then selectExport.
- InExport Device Configuration, complete the following steps:
- In theConfig fileview, selectExport. The file exports to your configured browser download location.
- (optional) If the device also requires a Vlan file, selectNext, then in theVlan fileview, selectExport. The file exports to your configured browser download location.
- SelectNext, then selectClose.
- SelectOK.
Provide Feedback