Device List
How do I open Device list?
- On the explorer bar, select
Devices. - InDevicesexplorer, selectDevice list.
TIP:
From the top toolbar, select
Device list
to open the Device list while in any explorer. Use
Device list
to:
- View, edit, and delete devices.
- Open the device properties.
- View tags and parameters for the devices in the project.
- Edit the Name, Description, and Minor revision of a device.
The
Device list
displays information for each device:Column | Description |
|---|---|
Name | Set the user-defined name of the device. |
Description | Set the user-defined description of the device. |
Revision | The firmware revision of the device. The major revision value is read-only, but you can set the minor revision value. |
Catalog Number | The catalog number of the device. Hover over the catalog number to view the catalog description. |
Category | The type of the device. |
Vendor | The manufacturer of the device. |
Electronic Keying | The electronic keying used for the module. Electronic keying compares the module defined in the project to the installed module. If keying fails, a fault occurs. Valid values are Exact Match, Compatible Module, and Disable Keying. For detailed
information on Electronic Keying, see Electronic Keying in Logix5000 Control Systems Application Technique, publication LOGIX-AT001.Electronic Keying options include:
|
TIP:
- To open the profile of a device, inDevice list, right-click the device and selectOpen device properties.Overviewview opens.
Provide Feedback