Delete a device
Delete a device to remove the device from a bus and the project. Devices connected to buses below the deleted device are disconnected and returned to the
Unassigned
folder in Device Explorer
.
TIP:
Any changes made to devices while online will only impact the offline project.
To delete a device
- On the explorer bar, select
Devices. - InDevices, right-click a device in the list, then select
Delete. The device is removed from the project.
NOTE:
When you delete a device, the devices assigned to it become unassigned, and on rack optimized devices, the device connection type reverts to the default setting, Data.
Provide Feedback