Delete a controller
Delete a controller to remove the controller from the project. The tasks, programs, and allocations to Smart Objects for the controller are removed with the controller. Devices attached to a backplane or bus of the controller are moved to the
Unassigned
folder. Delete a controller from the Devices
explorer.To delete a controller
- On the explorer bar, select
Devices. - InDevicesexplorer, right-click the controller and select
Delete.
The controller is removed.
TIP:
You have the option to delete a controller from the
Device list
by selecting Device list
under the Devices explorer, right-clicking a controller in the Device list
tab, and selecting 
Delete
.Provide Feedback