Launch the Unit Profile from the IntelliCENTER explorer
Use the
Unit Profile
tab to view detailed unit information in the IntelliCENTER lineup. View the:
- device name
- device type
- IP address
- MCC Network number
- vendor code
- product type
- product code
- major revision
- minor revision
To launch the Unit Profile from the IntelliCENTER explorer
- On the explorer bar, select
Devices. - Select theIntelliCENTERtab.
- In theIntelliCENTERexplorer, right-click a unit within a lineup and selectUnit Profileto launch the Unit Profile and to view the unit information.
- (optional) To view unit documentation, underDocumentation, select theDrawings,Manuals, orSpareslink.
Provide Feedback