Export an MCC lineup
Export an MCC lineup to use the lineup in the local install of IntelliCENTER.
To export an MCC lineup
- From the main menu, open or create a project that contains an MCC lineup.
- SelectFile > Export MCC lineupto open theExport MCC Lineupdialog box.
- SelectExportto add the MCC lineup to a zip file. When the lineup has zipped successfully, theExport MCC Lineupdialog box opens.
- SelectDownloadto download the zipped dataset to the computer'sDownloadsfolder.
- Download theupdate_datasetfile.
- Copy the file to the original dataset folder.
- RunUpdate_dataset.exeas an admin.
- If this is the first time you are installing the dataset on your computer, leave theDestination folder of Database filesas the default. If the lineup is already installed on your computer, select a new location for the database and documentation.
- Restart your computer and open the IntelliCENTER software version six to access the dataset containing the changes you made in FactoryTalk Design Studio.Other ways to export an MCC lineup:
- From the IntelliCENTER dashboard by selecting the box
associated with the lineup to export and then selecting the Export lineupoption. For information on how to access the IntelliCENTER dashboard, see IntelliCENTER Dashboard. - In the IntelliCENTER explorer, either right-click the name of the MCC lineup or a blank space within the explorer and then selectExport MCC lineup.
- In theElevationview, right-click a blank area within the view and then selectExport MCC lineup. For more information about theElevationview, see Elevation view.
Provide Feedback