Update the definition of a FactoryTalk Smart Object from an instance
Update the definition of a
FactoryTalk Smart Object
from an instance in the System
explorer to update the instances of the FactoryTalk Smart Object
and the definition of the FactoryTalk Smart Object
in the Library
.
IMPORTANT:
Modifying FactoryTalk Smart Objects using the Code Editor may result in syntax errors that will prevent the explorers from displaying information. We recommend using the user interface to create or modify FactoryTalk Smart Objects.
- On the explorer bar, select
System. - Right-click aFactoryTalk Smart Objectand selectUpdate definition.
- InUpdate definition, view the list of instances and definitions affected by any updates to the definition and then change:
- Name. The name ofFactoryTalk Smart Object.
- Description. An optional description of what theFactoryTalk Smart Objectlogic does in the system.
- New version number. Assign a version number from 1 to 999.TIP: You can change the name of the definition inPropertiesinSmart Object definition.
- SelectUpdate definition.
Provide Feedback