Remove a FactoryTalk Smart Object instance from the definition
Remove
FactoryTalk Smart Object
instance from the definition to no longer have the instance update when modifying the definition of the FactoryTalk Smart Object
. Removing the instance of a FactoryTalk Smart Object
from the definition removes all associated FactoryTalk Smart Object
from the definition. This makes the FactoryTalk Smart Object
instance a standalone FactoryTalk Smart Object
.
IMPORTANT:
Modifying FactoryTalk Smart Objects using the Code Editor may result in syntax errors that will prevent the explorers from displaying information. We recommend using the user interface to create or modify FactoryTalk Smart Objects.
- On the explorer bar, select
System. - Right-click theFactoryTalk Smart Objectinstance and selectRemove instance from definition.
- SelectRemove. The instance is no longer associated with the definition.
Provide Feedback