Override a program of an instance
Use override to change or update the content in a Smart Object program.
- On the explorer bar, select
System, expand theFactoryTalk Smart Objectthat is an instance of a definition, and then right-click a program. - SelectOverride program. A copy of the program replaces the original program.
TIP:
If selecting
Copy content
for an override, any changes to a tag value or property or a program and routine property is saved in the copy of the program. If you do not select Copy content
, the resulting program, and the program content, is removedProvide Feedback